question related IFC Pins shifting T1042

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

question related IFC Pins shifting T1042

653件の閲覧回数
faizmajeed
Contributor III

Hi!

I have question related IFC Pins shifting. According to reference manual of T1042 Section : 24.4.1.2.1

"In this mode of muxing, the IFC supplies the most significant bit (msb) of the address bits
on the AD bus."

and they provided a picture i attached. now in reference schematics, there is some difference in pins assignment that instead of making AD0 as MSB, they have connected IFCA5 on MSB address bit of flash.

What are your recommendation that how we should connect it.

Thanks 

Manual_Snap.PNG

Schematics Snap.PNG#

タグ(2)
0 件の賞賛
返信
1 返信

603件の閲覧回数
r8070z
NXP Employee
NXP Employee

The Figure 24-9 is not suitable for the T1042/T1040. It is for processor which provides the least significant address bit on pin named A26 in the mode 0. The T1042 does that on pin named IFC_A31 in this mode. The second picture looks like T1040RDB schematics where IFC_A[31:16] come from the T1042 IFC_A[31:16] and IFC_A[15:8], IFC_VA[7:5] are latched  from the T1042 IFC_AD[15:05]. It is correct for ADM mode 0

0 件の賞賛
返信