hello all,
There are few signals namely PS_VTT_EN and PS_VTT_PG_B which are connected only to CPLD and found no where else. What do they actually mean?
And also where is SD1REFCLK_SEL signal taken from Dip swicth going? Please clarify?
Thanks in Advance
Urmila P.
已解决! 转到解答。
PS_VTT_EN and PS_VTT_PG_B were intended to be used if a separate chip is used to generate VTT voltage for DDR4 memory interface. Since the VTT is generated on the same chip alone with DDR VDD (GVDD), PS_VTT_EN and PS_VTT_PG_B signals are not used on the board.
SD1REFCLK_SEL from the switch goes to the CPLD and to U31 clock source. It selects SD1_REFCLK2 clock frequency between 100MHz and 156.25MHz.
Regards,
Bulat
PS_VTT_EN and PS_VTT_PG_B were intended to be used if a separate chip is used to generate VTT voltage for DDR4 memory interface. Since the VTT is generated on the same chip alone with DDR VDD (GVDD), PS_VTT_EN and PS_VTT_PG_B signals are not used on the board.
SD1REFCLK_SEL from the switch goes to the CPLD and to U31 clock source. It selects SD1_REFCLK2 clock frequency between 100MHz and 156.25MHz.
Regards,
Bulat
CPLD's SD1REFCLK_SEL pin is an input-output signal. At power up it acts as an input, fetches voltage level from the DIP switch, stores the value in the REG_SD1REFCLK_SEL register (see board Ref Manual). Then it becomes an output and drives the value stored in the register.
Regards,
Bulat