lsdk flex-builder fails to build

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

lsdk flex-builder fails to build

987件の閲覧回数
holder
Contributor I

I am using LSDK flexbuild1809 on Ubuntu 18.04 running in a VirtualBox VM.

My target is LS1088ARDB.

I run the following command:

flex-builder -m ls1088ardb -a arm64 -b sd

The build fails with the following error:

...

INSTRUCTION: mkbootpartition
DESTARCH: arm64
SECURE: y
CONFIGLIST: build_lsdk.cfg
INSTRUCTION: mklinux
DESTARCH: arm64
CONFIGLIST: build_lsdk.cfg
umount: /home/boeing/lsdk1809/flexbuild_lsdk1809/packages/rfs/ramdiskrfs/mntrd: target is busy.

I have to restart the build again which completes w/o error.

Any suggestions on the above "umount" error?

bob

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

657件の閲覧回数
holder
Contributor I

I updated VirtualBox from 5.2.18 to 5.2.20.

I repeated the above build command and did not see the error.

0 件の賞賛
返信

657件の閲覧回数
Pavel
NXP Employee
NXP Employee

We use Ubuntu 18 Linux or Ubuntu 18 virtual VmWare machine for LSDK using.

There is no problem for building if Ubuntu 18 64bit is used.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信