ls1046 timestamp

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

ls1046 timestamp

571 次查看
kwangholee
Contributor I
Hi dear.
Does the ieee1588 timestamp function work on both Serdes1 Lane1 (SFP), Serdes 1 Lane0 (10g / 2.5g rj46), EC1 to EC4 on the LS1046?
0 项奖励
1 回复

500 次查看
bpe
NXP Employee
NXP Employee


IEEE1588 timestamping unit is part of mEMAC which is behind SerDes or parallel
interface and works independently of the connection type or data rate.

Regards,

Platon

0 项奖励