how to use qspi_b in LS1046a

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to use qspi_b in LS1046a

Jump to solution
2,022 Views
yenchao
Contributor IV

Hi,

I have a ls1046a carrier board and would like to use QSPI_B (used as SPI, i.e., only QSPI_B_SCK, QSPI_B_DATA0 and QSPI_B_DATA1 are used) to connect mcp2518fd(spi to can controller).

It seems like &qspi in fsl-ls1046a-rdb.dts is QSPI_A, so how to configure QSPI_B?

Thx

Yen

0 Kudos
Reply
1 Solution
1,782 Views
yenchao
Contributor IV

Hi

The answer is 

- reg: There are two buses (A and B) with two chip selects each.
This encodes to which bus and CS the flash is connected:
<0>: Bus A, CS 0
<1>: Bus A, CS 1
<2>: Bus B, CS 0
<3>: Bus B, CS 1

 

Thx

Yen

View solution in original post

0 Kudos
Reply
12 Replies
2,002 Views
yenchao
Contributor IV

Hi NXP,

 

Any advices?

 

Thx

Yen

0 Kudos
Reply
1,972 Views
Chavira
NXP TechSupport
NXP TechSupport

Yes. It is possible to connect two QSPI in the LS1046A.
Actually, LS1046A can work with up to 4 flashes as you already pointed to the CS.
The qSPI boot, however, has to boot from qSPI A, which uses SPI_A_CS0. Whether you want to connect the 2nd flash to which one, really depends on customer design. You can connect to any of the 3 CSs. The DTS file has to match the hardware design.

0 Kudos
Reply
1,969 Views
yenchao
Contributor IV

Hi,

I would like to know where to add mcp2518fd node in fsl-ls1046a-rdb.dts.

Is this correct?

&qspi {
	status = "okay";
// added by Yen for mcp2518fd	
        can@2 {
            compatible = "microchip,mcp2518fd";
            reg = <2>;
            clocks = <&mcp2518fd_osc>;
//            pinctrl-names = "default";
//            pinctrl-0 = <&can0_pins>;
            spi-max-frequency = <20000000>;
//            interrupts-extended = <&gpio 13 IRQ_TYPE_LEVEL_LOW>;
            microchip,rx-int-gpios = <&gpio1 27 GPIO_ACTIVE_LOW>;
            vdd-supply = <&sb_3v3>;
//            xceiver-supply = <&reg5v0>;
        };	
////
};

If yes, how can I assign it to QSPI_B?

If I am wrong, please advice where to add mcp2518fd node and assign it to QSPI_B.

 

Thx

Yen

0 Kudos
Reply
1,957 Views
yenchao
Contributor IV

Hi

Any updates for how to add mcp2518fd node into device tree?

Thx

Yen

0 Kudos
Reply
1,949 Views
Chavira
NXP TechSupport
NXP TechSupport

Please refer to arch/arm64/boot/dts/freescale/fsl-ls1046a-rdb.dts and arch/arm64/boot/dts/freescale/fsl-ls1046a-rdb.dts and fsl-ls1046a.dtsi. In the later file, it already defined following:


qspi: spi@1550000 {
compatible = "fsl,ls1021a-qspi";
#address-cells = <1>;
#size-cells = <0>;
reg = <0x0 0x1550000 0x0 0x10000>,
<0x0 0x40000000 0x0 0x10000000>;
reg-names = "QuadSPI", "QuadSPI-memory";
interrupts = <GIC_SPI 99 IRQ_TYPE_LEVEL_HIGH>;
clock-names = "qspi_en", "qspi";
clocks = <&clockgen 4 1>, <&clockgen 4 1>;
status = "disabled";
};
In the first file, a specific flash device can be defined as following example.
s25fs512s1: flash@1 {
compatible = "jedec,spi-nor";
#address-cells = <1>;
#size-cells = <1>;
spi-max-frequency = <50000000>;
spi-rx-bus-width = <1>;
spi-tx-bus-width = <1>;
reg = <1>;
};


On LS1046A, qSPI interface only support 1.8V.
By the way, I could be wrong, I do not recommend to use qSPI to connect mcp2518fd. The SPI interface would be proper for this device.

0 Kudos
Reply
1,922 Views
yenchao
Contributor IV

Hi

We have a voltage level translator, so the voltage is not a problem.

Please advise how to assign mcp2158fd node to QSPI_B.

(It seems like default is QSPI_A)

Thx

Yen

0 Kudos
Reply
1,916 Views
Chavira
NXP TechSupport
NXP TechSupport

You can manage two QSPI from node A because we have two chip selects in node A.

We can be sure if that memory can work due to the level Voltage, I know that issue was resolved with level shifters but originally the memory is not supported for the MPU.

0 Kudos
Reply
1,900 Views
yenchao
Contributor IV

Hi,

We would like to add mcp2518fd to QSPI node B, not node A.

Please help us how to assign mcp2518fd to QSPI node "B" in dts file

 

Thx

Yen

0 Kudos
Reply
1,884 Views
Chavira
NXP TechSupport
NXP TechSupport

It can be either A or B. The register settings in qSPI_SFxyAD determined the memory location. Therefore, qSPI controller will access proper flashes if SW gives a valid location according to where this location address resides in which flash memory range.

0 Kudos
Reply
1,871 Views
yenchao
Contributor IV

Hi

Is this correct for assigning mcp158fd to QSPI_B in fsl-ls1046a-rdb.dts?

&qspi {
	status = "okay";

	s25fs512s0: flash@0 {
		compatible = "jedec,spi-nor";
		#address-cells = <1>;
		#size-cells = <1>;
		spi-max-frequency = <50000000>;
		spi-rx-bus-width = <1>;
		spi-tx-bus-width = <1>;
		reg = <0>;
	};

	s25fs512s1: flash@1 {
		compatible = "jedec,spi-nor";
		#address-cells = <1>;
		#size-cells = <1>;
		spi-max-frequency = <50000000>;
		spi-rx-bus-width = <1>;
		spi-tx-bus-width = <1>;
		reg = <1>;
	};
	
// added by Yen for mcp2518fd	
        can@2 {
		compatible = "microchip,mcp2518fd";
		reg = <2>;
		clocks = <&mcp2518fd_osc>;
		spi-max-frequency = <20000000>;
                microchip,rx-int-gpios = <&gpio1 27 GPIO_ACTIVE_LOW>;
		vdd-supply = <&sb_3v3>;
		xceiver-supply = <&sb_5v0>;			
        };	
////	
};

 

0 Kudos
Reply
1,853 Views
yenchao
Contributor IV

Hi

Any updates?

Thx

Yen

0 Kudos
Reply
1,783 Views
yenchao
Contributor IV

Hi

The answer is 

- reg: There are two buses (A and B) with two chip selects each.
This encodes to which bus and CS the flash is connected:
<0>: Bus A, CS 0
<1>: Bus A, CS 1
<2>: Bus B, CS 0
<3>: Bus B, CS 1

 

Thx

Yen

0 Kudos
Reply