flexCan pins for tx and rx

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

flexCan pins for tx and rx

737 Views
hittzt
Senior Contributor I

Hi exports,

When I test nxp-ls1028ardb board, the I did not get the pins of flexCan for tx, rx and ground in docs of nxp-ls1028 including user maunal, reference manual etc.

Would you please give the pin info about flexcan on nxp-ls1028 of schematic of nxp-ls1028?

Thanks,

Zhantao

0 Kudos
Reply
4 Replies

647 Views
ufedor
NXP Employee
NXP Employee

CAN signals are multiplexed with other functions - refer to the QorIQ LS1028A/LS1018A Data Sheet, Table 1. Pinout list by bus:

CAN.jpg

The multiplexing is controlled by the RCW fields - refer to the QorIQ LS1028A Reference Manual, 4.8.8.7 Reset Control Word (RCW) Register Descriptions:

CAN_RCW.jpg

0 Kudos
Reply

647 Views
hittzt
Senior Contributor I

Hi ufedor,

Thanks for your reply.

Is there any diagram or table for 9 pins distribution of CAN interface.

Thanks,

Zhantao

0 Kudos
Reply

647 Views
ufedor
NXP Employee
NXP Employee

CAN.jpg

0 Kudos
Reply

647 Views
hittzt
Senior Contributor I

Hi ufedor,

 

Thanks for your reply.

Thanks

Zhantao

0 Kudos
Reply