Hello everyone,
I'm beginning to use an LS2088ARDB board and I'm trying to use it with pktgen from dpdk.
I managed to have ports generate frames when i use 1,2 or 3 ports but it fails when I use more.
I start by creating a dprc containing my 4 dpni/dpmac using the "dynamic_dpl.sh" script, then i export DPRC=dprc.2 and i launch the application:
pktgen -l 0-7 -n 8 --proc-type auto --file-prefix pg --log-level 8 -- -T -P -m "1.0,2.1,3.2,4.3" -l pktgentest.log
that command fails with messages:
mempool/dpaa2: DPAA2 pool not available!
mempool/dpaa2: Not a valid dpaa2 buffer pool
!PANIC!: Cannot create mbuf pool (Default TX 3:0) port 3, queue 0, nb_mbufs 8192, socket_id 0: No such file or directory
PANIC in pktgen_mbuf_pool_create():
Cannot create mbuf pool (Default TX 3:0) port 3, queue 0, nb_mbufs 8192, socket_id 0: No such file or directory1: [pktgen(rte_dump_stack+0x38) [0xaaaae5a207b8]]
while the command:
pktgen -l 0-7 -n 8 --proc-type auto --file-prefix pg --log-level 8 -- -T -P -m "1.0,2.1,3.2" -l pktgentest.log
works fine.
The board should be able to handle that 4th port using a 4th core in my opinion.
I'm begining to use the platform and i have not fully understood the architecture.
Does anyone have an idea about this issue?
Thanks
已解决! 转到解答。
Please refer to the following example, please change DPBP_COUNT value.
root@lx2160ardb:/usr/share/dpdk/dpaa2# export DPBP_COUNT=36
root@lx2160ardb:/usr/share/dpdk/dpaa2# ./dynamic_dpl.sh dpmac.3 dpmac.4 dpmac.5 dpmac.6
export DPRC=dprc.2
Please refer to the following example, please change DPBP_COUNT value.
root@lx2160ardb:/usr/share/dpdk/dpaa2# export DPBP_COUNT=36
root@lx2160ardb:/usr/share/dpdk/dpaa2# ./dynamic_dpl.sh dpmac.3 dpmac.4 dpmac.5 dpmac.6
export DPRC=dprc.2