we use flexbuild_lsdk1909_update_311219.tgz , and auto download and build , do as blelow:
1 source setup.env
flex-builder -m lx2160ardb -a arm64
2 then done successfully, but firmware_lx2160ardb_uboot_sdboot.img of build is only 27.9M, bootpartition_LS_arm64_lts_4.19.tgz is only 45.2M, rootfs_lsdk1909_LS_arm64_main.tgz is only 702M,
then I build them in SD card,
" flex-installer -b bootpartition_LS_arm64_lts_4.19.tgz -r rootfs_lsdk1909_LS_arm64_main.tgz -f firmware_lx2160ardb_uboot_sdboot.img -d /dev/sdx ",
and lx2160ardb board Uboot run, at Uboot , I run cmd "run sd_bootcmd" , run fail....
3 I get firmware_lx2160ardb_uboot_sdboot.img from NXP.COM, the size is 45.6M,
I get bootpartition_LS_arm64_lts_4.19.tgz from NXP.COM, the size is 366M,
I get rootfs_lsdk1909_LS_arm64_main.tgz from NXP.COM, the size is 728M,
then I build them in SD card, and lx2160ardb board Uboot run, at Uboot , I run cmd "run sd_bootcmd" , run successfully....
4 why the three file I build is low size, size is not true ?? i build them at ubuntu 18.04. any other steps need to be done ??
5 Yiping Wang answer that " remove build folder and rebuild your images." , I use command "flex-builder -i mkfw -m lx2160ardb -b sd" , but firmware_lx2160ardb_uboot_sdboot.img of build is also 27.9M .
6 the attach file log1 is log of my build, but no error
Usually it happens if different versions of LSDK are used.
See attached snapshot. It is result of image building using LSDK 2004.
NXP recommends using LSDK 2004 for the LX2160a:
Have a great day,
Pavel Chubakov
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------