bringing up LS1088A custom board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

bringing up LS1088A custom board

340 Views
p_dembicki
Contributor II

Hi everybody,

I'm struggling with custom LS1088A board. It has ddr4 module (so-dimm in my case) and it use only one diff clock: 100Mhz. There no additional clocks for DDR or SERDES. I try to boot it from SD-CARD.

 

My problem is simple: board cannot start. Please look at screen:

003.png

 

Yellow is PORESET_B, Blue is HRESET_B, Green is RESETREQ_B and pink is ASLEEP. All signals are pulled up.

Second image:
004.png

 

Green RESET_REQ_B, blue HRESET_B, pink SDCARD_D0, yellow SD_CARD_CMD.

It looks like cpu fail at 18 step of Power-On Reset Sequence. And I can't force it to start up.

My RCW settings:

#include <ls1088rdb.rcwi>

SYS_PLL_RAT=5
MEM_PLL_RAT=16
CGA_PLL1_RAT=12
CGA_PLL2_RAT=12
HWA_CGA_M1_CLK_SEL=2
HWA_CGA_M2_CLK_SEL=1
DDR_REFCLK_SEL=2
DRAM_LAT=1
BOOT_LOC=21
FLASH_MODE=0x2
SYSCLK_FREQ=0x258
IIC3_EXT=1
UART_BASE=3
IIC2_BASE=2
IIC3_BASE=1
IIC4_BASE=1
IFC_GRP_A_BASE=3
IFC_GRP_FGHI_BASE=1
EC1=1
EC2=1
USB1_CLK_FSEL=39
USB2_CLK_FSEL=39
SRDS_PLL_PD_PLL2=1
SRDS_PLL_PD_PLL4=1
SRDS_PRTCL_S1_LN0=3
SRDS_PRTCL_S1_LN1=3
SRDS_PRTCL_S1_LN2=4
SRDS_PRTCL_S1_LN3=4
SRDS_PRTCL_S2_LN0=5
SRDS_PRTCL_S2_LN1=5
SRDS_PRTCL_S2_LN2=7
SRDS_PRTCL_S2_LN3=7
SRDS_DIV_PEX_S2=2
SRDS_S1_REFCLK_SRC_SEL=3
SRDS_S2_REFCLK_SRC_SEL=3

.pbi
blockcopy 0x40,0x00100000,0x1800a000,0x00015000
.end
#include <bootlocptr_sdhc.rcw>
#include <a009102_single.rcw>
#include <a010554_single.rcw>
#include <a009531.rcw>
#include <tcpz_nosecure_region.rcw>
/* CRC and Stop command (CRC 0x90c59bb0)*/


SD-Card with the same image boot inserted to LS1088A-RDB.

My question is:
What could be wrong?
How can I debug that issue?
Could You help me please? 

BR,
Pawel


Labels (1)
Tags (1)
0 Kudos
5 Replies

252 Views
LFGP
NXP TechSupport
NXP TechSupport

The problem is in RAM, please be sure the DDRA SODIMM is supported and double check signals and clocks you are using.

The frozen issue is due some problem in RAM.

0 Kudos

292 Views
LFGP
NXP TechSupport
NXP TechSupport

there's could be several thing to provoque DDR issues, please use the next link in order to get the check list for DDR,

https://community.nxp.com/pwmxy87654/attachments/pwmxy87654/imx-processors/188384/1/AN5097.pdf 

Majority of the customer DDR issues can be resolved by:
• Schematics review for any errors
• Verify DRAM reset signal is correct
• Use the QCVS tool to generate and validate DDR
• Verify DQ mapping is correct
• Verify write leveling by entering correct CLK to DQS skew in QCVS
tool

also please check the doc in the next link,

https://community.nxp.com/pwmxy87654/attachments/pwmxy87654/tech-days/289/1/AMF-NET-T3267.pdf 

0 Kudos

272 Views
p_dembicki
Contributor II
Thank you for the interesting topic.

I tried to bring up the devboard with an unconnected DDR4 UDIMM, and it started. After that, it displayed an SPD read error on the console and froze. However, it did start. My board didn't display anything on the console and remained in the ASLEEP state.

So, my board with the same image should output something on the serial console, but it remained silent.
0 Kudos

251 Views
LFGP
NXP TechSupport
NXP TechSupport
The problem is in RAM, please be sure the DDRA SODIMM is supported and double check signals and clocks you are using.

The frozen issue is due some problem in RAM.
0 Kudos

219 Views
p_dembicki
Contributor II
Please advise: How can I adjust the CodeWarrior init script to utilize DIFF_SYSCLK as the DDR source clock in safeRCW mode? I use DIFF_SYSCLK as only source clock for everything.

At this moment my init script fail in safercw mode:
"Failed to write memory at address 0x70007002c on core CortexA53#0."
0 Kudos