Attempting to select mirror byte function for error injection. ECC_ERR_INJECT[EMB, EIEN]= 0b'11
The default is 0b'00.
Why does writing to ECC_ERR_INJECT[EMB,EIEN]=0b'11 cause a reset?
root@ls1043ardb:~# devmem 0x1080E08 w 0x00030000
[ 839.465065] Unhandled fault: synchronous external abort (0x96000210) at 0xff
Then the WDT is triggered and the board resets.
I had someone check the byte ordering and it looks fine. If I set the EMB only or the EIEN without EMB set (0x00020000 or 0x00010000), there is no hard reset. Only when I set both the EMB,EIEN (0x00030000) does it do a hard reset.
22 EMB
ECC Mirror Byte.
0b - Mirror byte functionality disabled.
1b - Mirror the most significant data path byte onto the ECC byte.
23 EIEN
Error Injection Enable.
0b - Error injection disabled.
1b - Error injection enabled. This applies to the data mask bits, the ECC mask bits, and the ECC
mirror bit. Note that error injection should not be enabled until the memory controller has been
enabled via DDR_SDRAM_CFG[MEM_EN].
Yes, it means the LS1043RDB board doesn't correct DDR memory errors because of lack of external ECC memory.
The following NXP boards provide ECC support: LS1043A-QDS, LS1046A-RDB.
Have a great day,
Andrei
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------