Where is the IFC and RTC drivers in uboot and the kernel in SDK 2.0 for LS1043?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where is the IFC and RTC drivers in uboot and the kernel in SDK 2.0 for LS1043?

887 Views
Gandalf-kern
Contributor IV

Where is the IFC and RTC drivers for u-boot and the kernel in SDK2.0 on LS1043ardB and do you have the data sheet and part supported by the IFC driver?

Is the RTC enabled and are the Watchdog timers being used on the ls1043ard dev boatd?

Labels (1)
Tags (1)
0 Kudos
1 Reply

678 Views
Pavel
NXP Employee
NXP Employee

Look at the Section 7.13 of the SDK 2.0-1701 documentation about RTC clock using in this BSP:

http://www.nxp.com/assets/documents/data/en/supporting-information/QORIQ-SDK-2.0-IC-REV0.pdf

 

See the Chapter 7.8 of this documentation about NOR Flash Device Driver User Manual.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos