Where is information on the codeaurora sunset and how to address build breaks?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Where is information on the codeaurora sunset and how to address build breaks?

ソリューションへジャンプ
818件の閲覧回数
gfine1
Contributor III

When attempting a build I ran into build breaks.

I then find out that codeaurora was sunsetted, and everything was moved to github. 

What would be the proper path to take to rebuild my BSPs so they point to the proper repo in github? 

Would a bitbake -c clean core-image-minimal work? or is there a less invasive fix? 

We build using yocto and the dunfell branch (because of EOL concerns) 

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 解決策
756件の閲覧回数
Oswalag
NXP TechSupport
NXP TechSupport

Please take a look in the following Post that also apply to layerscape devices

Linux source code migration (CAF -> Github) - NXP Community

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
757件の閲覧回数
Oswalag
NXP TechSupport
NXP TechSupport

Please take a look in the following Post that also apply to layerscape devices

Linux source code migration (CAF -> Github) - NXP Community

0 件の賞賛
返信