Unable to configure regulatory domain for wireless network devices.[LS1046 6.1.55]

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Unable to configure regulatory domain for wireless network devices.[LS1046 6.1.55]

ソリューションへジャンプ
573件の閲覧回数
HiroakiOkoshi
Contributor III

I'm using ls1046afrwy-yocto-6.1.55-2.2.0. I am changing CFG80211 to module, but I cannot set the regulatory domain for the wireless network device. Is there anything else I should be careful about?

 

root@ls1046afrwy:/run/media/FAT-sda1/jody-w6# uname -a

Linux ls1046afrwy 6.1.55+g770c5fe2c1d1 #1 SMP PREEMPT Tue Nov 21 23:45:58 UTC 2023 aarch64 GNU/Linux

root@ls1046afrwy:/run/media/FAT-sda1/jody-w6# iw reg set JP

root@ls1046afrwy:/run/media/FAT-sda1/jody-w6# iw reg get
global
country 00: DFS-UNSET
(2402 - 2472 @ 40), (6, 20), (N/A)
(2457 - 2482 @ 20), (6, 20), (N/A), AUTO-BW, PASSIVE-SCAN
(2474 - 2494 @ 20), (6, 20), (N/A), NO-OFDM, PASSIVE-SCAN
(5170 - 5250 @ 80), (6, 20), (N/A), AUTO-BW, PASSIVE-SCAN
(5250 - 5330 @ 80), (6, 20), (0 ms), DFS, AUTO-BW, PASSIVE-SCAN
(5490 - 5730 @ 160), (6, 20), (0 ms), DFS, PASSIVE-SCAN
(5735 - 5835 @ 80), (6, 20), (N/A), PASSIVE-SCAN
(57240 - 63720 @ 2160), (N/A, 0), (N/A)

root@ls1046afrwy:/run/media/FAT-sda1/jody-w6# dmesg | grep X.5
[ 6.625048] Loading compiled-in X.509 certificates
[ 12.516070] cfg80211: Loading compiled-in X.509 certificates for regulatory database
[ 12.531607] cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'

root@ls1046afrwy:/run/media/FAT-sda1/jody-w6# lsmod
Module Size Used by
pciexxx 782336 6
mlan 548864 1 pciexxx
cfg80211 425984 1 pciexxx
rfkill 32768 8 cfg80211
fsl_jr_uio 16384 0
caam_jr 217088 0
caamkeyblob_desc 16384 1 caam_jr
caamhash_desc 16384 1 caam_jr
caamalg_desc 36864 1 caam_jr
crypto_engine 20480 1 caam_jr
libdes 24576 1 caam_jr
fsl_qdma 24576 0
pci_endpoint_test 20480 0
at24 20480 0
ina2xx 16384 0
lm90 36864 0
rtc_fsl_ftm_alarm 16384 1
rtc_pcf2127 20480 0
caam 36864 1 caam_jr
nvmem_layerscape_sfp 16384 0
layerscape_edac_mod 20480 0
error 24576 6 caamalg_desc,caamkeyblob_desc,caamhash_desc,caam,caam_jr,fsl_jr_uio
crct10dif_ce 16384 1

Best Regards

Hiroaki Okoshi

 

0 件の賞賛
返信
1 解決策
554件の閲覧回数
HiroakiOkoshi
Contributor III
0 件の賞賛
返信
2 返答(返信)
555件の閲覧回数
HiroakiOkoshi
Contributor III
0 件の賞賛
返信
438件の閲覧回数
javadR3
Contributor III

Hi,

Because certificate(public/private key) has been changed in the latest wireless-regdb. You need to include the new certificate in your kernel.

Regards,

Javad

0 件の賞賛
返信