Hi:
I am compiling Ubuntu mate using lsdk2012, but there is no desktop. When installed on the custom board, only the display cursor flashes,I checked the service list and found that some services failed.Please refer to the services marked in red. Is there any impact?
networking.service loaded active exited Raise network inte>
● NetworkManager-wait-online.service loaded failed failed Network Manager Wa>
NetworkManager.service loaded active running Network Manager >
openvpn.service loaded active exited OpenVPN service >
polkit.service loaded active running Authorization Mana>
systemd-journal-flush.service loaded active exited Flush Journal to P>
systemd-journald.service loaded active running Journal Service >
systemd-logind.service loaded active running Login Service >
systemd-modules-load.service loaded active exited Load Kernel Module>
systemd-networkd-wait-online.service loaded active exited Wait for Network t>
systemd-networkd.service loaded active running Network Service >
systemd-random-seed.service loaded active exited Load/Save Random S>
systemd-remount-fs.service loaded active exited Remount Root and K>
systemd-resolved.service loaded active running Network Name Resol>
systemd-sysctl.service loaded active exited Apply Kernel Varia>
systemd-sysusers.service loaded active exited Create System User>
systemd-timesyncd.service loaded active running Network Time Synch>
systemd-tmpfiles-setup-dev.service loaded active exited Create Static Devi>
systemd-tmpfiles-setup.service loaded active exited Create Volatile Fi>
systemd-udev-trigger.service loaded active exited udev Coldplug all >
systemd-udevd.service loaded active running udev Kernel Device>
systemd-update-utmp.service loaded active exited Update UTMP about >
systemd-user-sessions.service loaded active exited Permit User Sessio>
udisks2.service loaded active running Disk Manager >
ufw.service loaded active exited Uncomplicated fire>
unattended-upgrades.service loaded active running Unattended Upgrade>
upower.service loaded active running Daemon for power m>
user-runtime-dir@0.service loaded active exited User Runtime Direc>
user-runtime-dir@110.service loaded active exited User Runtime Direc>
user@0.service loaded active running User Manager for U>
user@110.service loaded active running User Manager for U>
● weston.service loaded failed failed Weston Wayland Com>
whoopsie.service loaded active running crash report submi>
wpa_supplicant.service loaded active running WPA supplicant >
In addition, mail_ DP is set to "Y" and been compiled into the kernel,not xx.ko file.
I discussed with the testing team, they didn't encounter this issue.
We compiled Ubuntu mate rootfs filesystem about 1.8G, please check whether you built ubuntu:mate rootfs completely.
In addition, the testing team suggest you use high speed SD card to verify ubuntu:mate rootfs.
Hi:
In addition, the Ubuntu mate I compiled is 1.7g. In addition, the Ubuntu mate I compiled is 1.7g. I can see that ilghtdm has been started, but there is no desktop
1.7G rootfs_lsdk2012_ubuntu_mate_arm64_202111102153.tgz
Please try this ubuntu:mate rootfs provided by the testing team
链接: https://pan.baidu.com/s/1jeOicHpgj3OLXBAdPgBfxQ 提取码: h4va
HI:
Thank you for your rootfs, but there is still no desktop, only cursor. I compiled the DP driver to the kernel, "mail-dp = y" instead of "mail-dp = M".Then start it manually, but complain that there is no GPU manager
root@ubuntu:~# /usr/sbin/lightdm
** (lightdm:1662): WARNING **: 00:02:04.543: Seat type 'xlocal' is deprecated, use 'type=local' instead
/sbin/prime-switch: 22: /usr/bin/gpu-manager: not found
Have your tried to use the pre-built image bootpartition_LS_arm64_lts_5.4.tgz?
wget https://www.nxp.com/lgfiles/sdk/lsdk2012/bootpartition_LS_arm64_lts_5.4.tgz