Hi All,
H/W: LS1021ATWR
SDK: v1.7
I have flashed the u-boot-ls1021atwr-lpuart.bin & rcw_1000_lpuart.bin to "BANK1" successfully ! But I am unable to get the u-boot console prompt since it is switching to HDMI by default, which shows u-boot console prompt on HDMI monitor rather than minicom. Even before setting video arguments ! Am I missing some thing ? Any hints are really appreciated.
LPUART U-boot from Bank1:
---------------------------------------------------------------------------------------------
=> tftp 81000000 u-boot_lpuart.bin
eTSEC1 Waiting for PHY auto negotiation to complete......... TIMEOUT !
eTSEC1: No link.
Speed: 100, full duplex
Using eTSEC2 device
TFTP from server 10.20.0.1; our IP address is 10.20.0.2
Filename 'u-boot.bin'.
Load address: 0x81000000
Loading: ##########################
1.7 MiB/s
done
Bytes transferred = 368336 (59ed0 hex)
=> tftp 82000000 rcw_1000.bin
Speed: 100, full duplex
Using eTSEC2 device
TFTP from server 10.20.0.1; our IP address is 10.20.0.2
Filename 'rcw_1000_lpuart.bin'.
Load address: 0x82000000
Loading: #
58.6 KiB/s
done
Bytes transferred = 120 (78 hex)
=> protect off all;erase 63f80000 63ffffff;cp.b 81000000 63f80000 80000
Un-Protect Flash Bank # 1
.... done
Erased 4 sectors
Copy to Flash... 9....8....7....6....5....4....3....2....1....done
=> protect off all;erase 64000000 6401ffff;cp.b 82000000 64000000 100
Un-Protect Flash Bank # 1
. done
Erased 1 sectors
Copy to Flash... 9done
=> reset
resetting ...
-----------------------------------------------------------------------------------
LPUART U-boot:
----------------------------------------------------------------------------------
U-Boot 2014.07-sdk-v1.7.x+g659b6a2 (Jan 30 2015 - 15:41:45)
CPU: Freescale LayerScape LS1021E, Version: 1.0, (0x87081110)
Clock Configuration:
CPU0(ARMV7):1000 MHz,
Bus:300 MHz, DDR:800 MHz (1600 MT/s data rate),
Reset Configuration Word (RCW):
00000000: 0608000a 00000000 00000000 00000000
00000010: 20000000 00407900 e0025a00 21046000
00000020: 00000000 00000000 00000000 08038000
00000030: 00080000 881b7340 00000000 00000000
Board: LS1021ATWR
CPLD: V2.3
PCBA: V4.0
VBank: 1
I2C: ready
DRAM: 1 GiB
Using SERDES1 Protocol: 32 (0x20)
Firmware 'Microcode version 0.0.1 for LS1021a r1.0' for 1021 V1.0
QE: uploading microcode 'Microcode for LS1021a r1.0' version 0.0.1
Flash: 128 MiB
MMC: FSL_SDHC: 0
EEPROM: CRC mismatch (89eb7bdd != ffffffff)
DCU: Switching to HDMI monitor @ 640x480
In: serial
Out: vga
Err: vga
<<<<< NO U-boot prompt // u-boot prompt is shown on HDMI monitor if connected.
-----------------------------------------------------------------------------------
Where do I need to make the change to get the u-boot prompt on minicom.. in LPUART mode ?
Hello srikanthkrishnakar,
Regarding the u-boot and RCW NOR Flash address.
First please switch to bank 0, then flash u-boot and RCW to alternate bank(bank 1) at bank 0.
Because the current bank u-boot treats the alternate bank u-boot and RCW at 0x63f80000 and 0x64000000.
Just remind you to flash image in the correct bank.
Have a great day,
Yiping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Yiping,
I followed the below mentioned steps:
To write u-boot & rcw to bank1:
ð tftp 81000000 u-boot_lpuart.bin
ð tftp 82000000 rcw_1000_dcw.bin
ð protect off all;erase 63f80000 63ffffff;cp.b 81000000 63f80000 80000
ð protect off all;erase 64000000 6401ffff;cp.b 82000000 64000000 100
Switch Settings:
SW[3.5]: ON Bank1
SW[3.5]:OFF Bank0 ( default )
Switching between NOR/SD:
SW[2.1]: OFF , SW[2.3]: ON, SD-BOOT
SW[2.1]: ON , SW[2.3]: OFF, NOR-BOOT
Do these steps looks OK ?
Thanks for your support!
Hello srikanth krishnakar,
According your u-boot log, your u-boot is generated on Jan 30 2015, but it seems that your purpose is flashing the pre_built image rcw_1000_lpuart.bin and u-boot-ls1021atwr_lpuart.bin on bank 1, so I suspect you didn't flash images on the correct bank.
1. Please configure the switch setting to configure the target as Bank0(default).
2. At bank0, flash images to bank1
tftp 81000000 u-boot-ls1021atwr_lpuart.bin
tftp 82000000 rcw_1000_lpuart.bin
protect off all;erase 63f80000 63ffffff;cp.b 81000000 63f80000 80000
protect off all;erase 64000000 6401ffff;cp.b 82000000 64000000 100
If I didn't get your purpose clearly, please feel free to let me know.
Have a great day,
Yiping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello Yiping,
Yes I followed the steps mentioned by you. Being at "Bank0" (default), flashed the latest "lpuart" variant of images (u-boot & rcw) and u-boot console prompt is available only on Bank0. I would like to know what is the purpose of "rcw_1000_sdboot.bin" has to be written, if in-case I am booting from SDCARD ?
I already have written "u-boot-with-spl-pbl.bin" image to SDCARD and able to see console prompt in SD_BOOT mode. But I am unable to identify that location where the "rcw_1000_sdboot.bin" should be written !!
Any pointers are really useful.
Quick note: Does the kernel have identical features and drivers supported in both NOR & SD Boot modes ? Or there are differences in features supported when we boot from SDCARD compared to NOR boot ?
Thanks in Advance!
Srikanth
Hello srikanth krishnakar,
Regarding your problem for LPUART boot from BANK 1, I have verified the prebuilt image on my target without any problem, please refer to my following steps.
1. Please check default switch setting.
LS1021A TWR X3
Switch 1 2 3 4 5 6 7 8
SW2 ON [1] OFF [0] OFF [0] OFF [0] ON [1] ON [1] ON [1] ON [1]
SW3 OFF ON ON OFF OFF OFF OFF ON
LS1021A TWR X2 Switch Setting
Switch 1 2 3 4 5 6 7 8
SW2 OFF [0] OFF [0] ON [1] OFF [0] OFF [0] ON [1] OFF [0] ON [1]
SW3 OFF ON ON OFF ON OFF OFF OFF
2. Boot the system from BANK 0, and flash lpuart image, I have attached for you, since I suspect there is problem with u-boot which you are using.
tftp 81000000 u-boot-ls1021atwr_lpuart.bin
tftp 82000000 rcw_1000_lpuart.bin
protect off all;erase 63f80000 63ffffff;cp.b 81000000 63f80000 80000
protect off all;erase 64000000 6401ffff;cp.b 82000000 64000000 100
3. Shorted the jumpers J19 & J20 to 1-2, and configure SW[3.5]: ON Bank1.
4. Power on the board, please refer to my log
U-Boot 2014.01Layerscape-SDK-V1.3+g50d6848 (Oct 24 2014 - 19:22:06)
CPU: Freescale LayerScape LS1021E, Version: 1.0, (0x87081110)
Clock Configuration:
CPU0(ARMV7):1000 MHz,
Bus:300 MHz, DDR:800 MHz (1600 MT/s data rate),
Reset Configuration Word (RCW):
00000000: 0608000a 00000000 00000000 00000000
00000010: 20000000 00407900 e0025a00 21046000
00000020: 00000000 00000000 00000000 08038000
00000030: 00080000 881b7340 00000000 00000000
Board: LS1021ATWR
CPLD: V2.3
PCBA: V4.0
VBank: 1
I2C: ready
DRAM: 1 GiB (DDR3, 32-bit, CL=10.5, ECC off)
Using SERDES1 Protocol: 32 (0x20)
Flash: 128 MiB
MMC: FSL_SDHC: 0
EEPROM: NXID v1
Firmware 'Microcode version 0.0.0 for T1040 r1.0' for 1040 V1.0
QE: uploading microcode 'Microcode for T1040 r1.0'
In: serial
Out: serial
Err: serial
SATA link 0 timeout.
AHCI 0001.0300 1 slots 1 ports ? Gbps 0x1 impl SATA mode
flags: 64bit ncq pm clo only pmp fbss pio slum part ccc
scanning bus for devices...
Found 0 device(s).
Net: eTSEC1 is in sgmii mode.
eTSEC2 is in sgmii mode.
eTSEC1 [PRIME], eTSEC2, eTSEC3
Hit any key to stop autoboot: 0
Actually I suspect you built u-boot with DCU enabled.
Have a great day,
Yiping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
u-boot-with-spl-pbl.bin already includes rcw for sdboot. rcw_1000_sdboot.bin is placed at the beginning of bin image. u-boot-with-spl-pbl.bin image includes rcw + pbi + uboot, so is a complete image for booting sd.
To create suck an image from the scratch refer to eSPI/SD/NAND Boot.
Adrian
Hello srikanthkrishnakar,
In your description, you didn't mention the switch setting, have you already configure "J19 and J20 short 1-2"?
You could refer to "Hardware Setting for Special Purposes" section in SDK document for the details.
Have a great day,
Yiping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------