Hello @all,
I'm writing to gather information needed to preform secure boot on LS1012A. LSDK User Guide contains information but is written in ambiguous fashion. There is no strict guide "how to" with steps.
UNDERSTANDING
2 ways of running secure boot:
QUESTIONS:
1. Please generate secure firmware image with the following command.
$ flex-builder -i mkfw -m ls1012ardb -b qspi -s
2. Flex-builder has already generated the whole secure firmware image including all images secure headers, you could deploy firmware_ls1012ardb_uboot_qspiboot_secure.img to the target board directly.
3. No need specific steps.
4. You could write OTPMK to fuse array under u-boot.
Write OTPMK fuse values on shadow registers
mw.l 1e80234 a29a0b2c
mw.l 1e80238 2c8cd201
mw.l 1e8023c 84027ca8
mw.l 1e80240 8e13c7b9
mw.l 1e80244 a0b9d347
mw.l 1e80248 50ef2622
mw.l 1e8024c 98a92efd
mw.l 1e80250 ed53d1c3
Check OTPMK_ZERO and OTPMK_SYNDROME as 0 in SecMon_HP Status Register
md 1e90014
80000900
Check SFP_SVHESR no parity error.
md 1e80024
00000000
Permanently write OTPMK from the mirror registers into the fuse array
mw 1e80020 0x02000000
Please program SRKH mirror registers in CodeWarrior CCS environment
ccs::config_server 0 10000
ccs::config_chain {ls1043a dap sap2}
display ccs::get_config_chain
#Check Initial SNVS State and Value in SCRATCH Registers
ccs::display_mem <dap position> 0x1e90014 4 0 4
ccs::display_mem <dap position> 0x1ee0200 4 0 4
#Wrie the SRK Hash Value in Mirror Registers
ccs::write_mem <dap position> 0x1e80254 4 0 <SRKH1>
ccs::write_mem <dap position> 0x1e80258 4 0 <SRKH2>
ccs::write_mem <dap position> 0x1e8025c 4 0 <SRKH3>
ccs::write_mem <dap position> 0x1e80260 4 0 <SRKH4>
ccs::write_mem <dap position> 0x1e80264 4 0 <SRKH5>
ccs::write_mem <dap position> 0x1e80268 4 0 <SRKH6>
ccs::write_mem <dap position> 0x1e8026c 4 0 <SRKH7>
ccs::write_mem <dap position> 0x1e80270 4 0 <SRKH8>
#Get the Core Out of Boot Hold-Off
ccs::write_mem <dap position> 0x1ee00e4 4 0 0x00000001
5. SB_EN is set during development stage.
Hi Yiping,
I am trying to study and deploy secure boot in LX2160ardb platform. I am not sure about some descriptions in the guide. Could you help to answer these questions?
1. I have no codewarrior at hand, so I add some new codes in bl2_main() fucntion. OPTMK/SRKH registers are written here. It looks work well. If don't care to rebuild bl2 bin file repeatedly, does this method have other potential issue?
2. For the SFP_INGR_REG (1e80020), though the guide says "after writing this register, Fuses will be burnt, which cannot be undo...", my test seems show that I can write to update OPTMK/SRKH register time and again. Is there something wrong in my operation? I always connect the "SFP Power" jumper(j9) in the board when doing test.
3. Where is the correct position to find the SRKH values? Currently I build the xxx_secure.img with flexbuild and then get the "SRK (Public Key) Hash" information after this build line "Header File Created: ./build/lx2160ardb/release/bl2_sd_sec.pbl". Then I write these SRK value to SRKH registers. Is this correct?
Thanks!
-Jerry