Is there any sample code for configuring p1010 L2SRAM as pure SRAM and executing program code from it?
Hi Sam
How are you intending to run the code for setting l2sram ?
I use a BDI3000 JTAG debugger and with it I can initialize
this as follows :
; Move the 256kB L2SRAM to the initial MMU page
WM32 0xFF720E44 0x0000001C ;L2ERRDIS: disable parity error
WM32 0xFF720000 0x50010000 ;L2CTL
WM32 0xFF720100 0xFFFC0000 ;L2SRBAR0: map to 0x0_FFFC0000
WM32 0xFF720104 0x00000000 ;L2SRBAREA0
WM32 0xFF720000 0x90010000 ;L2CTL
;
; load and execute some boot code
WM32 0xfffffffc 0x48000000 ;loop
EXEC 0xfffffffc
Perhaps this gives you an idea and you can transform it
to your usage.
Regards
Sinan Akman
Hi Sinan,
Thank you for your reply. I intend to run the code in the spl.s program, in the section prior to where spl copies itself from NAND to RAM and continues execution. Presently it is written to copy itself to SDRAM, I want it to execute from SRAM instead. I will translate your sample to the equivalent syntax and report back the results.
Kind regards,
Sam
Hi Sam
I am not sure which spl.s you are referring to but if
you like you can find the spl code that does this
in mainline u-boot/arch/powerpc/cpu/mpc85xx/spl_minimal.c
Look at the section enabled with CONFIG_SYS_INIT_L2_ADDR.
Hope this helps
Regards
Sinan Akman
Hi Sam
OK so this is from VxWorks. The code should
work there as well, you just need to make sure
it lined up well with the address space it is setting
and that there is no clash for L2SRAM.
Regards
Sinan Akman