Request for Firmware that is programmed to MK20DX128VFM5 IC in FRW-LS1012A.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Request for Firmware that is programmed to MK20DX128VFM5 IC in FRW-LS1012A.

27 Views
annonymous_user
Contributor II

Hello,

I am currently working on a custom board design that incorporates the MK20DX128VFM5 IC, similar to its use in the FRWY-LS1012A board.

Specifically, I require the firmware that enables the MK20DX128VFM5 to function as it does in the FRWY-LS1012A evaluation board.

Could anyone provide this firmware or direct me to a source where I can obtain it? Additionally, if there are any specific configuration or setup guidelines for this firmware, as well as instructions on how to program the MK20DX128VFM5 with the provided firmware, that information would be highly appreciated.

Thank you in advance for your assistance!

Best Regards,

Dhanyalakshmi K N

0 Kudos
Reply
0 Replies