Raw SerDes Usage on LX2160A

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Raw SerDes Usage on LX2160A

跳至解决方案
750 次查看
reyesc
Contributor I

Hopefully this isn't too broad of a question (and is in the appropriate place).

I'm currently investigating transferring raw data via SerDes and was hoping someone could point me to some documentation/resources that might help out. Churning through the available docs I see that it's tied pretty tightly to the various protocols (ethernet, pcie, sata, etc) via dpaa2 and I haven't seen much in terms of utilizing the SerDes sans-protocol.

The use case here is pretty basic. At some point in the future the plan is to utilize the 25G and PCIe lanes, however currently the hardware won't be in place and so I'd just like to send some raw data out to verify our connections to those paths coming out of the chip. Basically, a loop-back test.

For what it's worth we're running LSDK 18.04.

Any help/info/guidance would be greatly appreciated. Let me know if more info is needed.

0 项奖励
回复
1 解答
665 次查看
yipingwang
NXP TechSupport
NXP TechSupport

There is a SerDes Validation tool which can be used to send raw data over the interface. You can loop back at near end or far end (if your link partner supports) and check if the bit stream is received correctly.

https://www.nxp.com/docs/en/user-guide/QCVS_SerDes_User_Guide.pdf
https://www.nxp.com/docs/en/application-note/AN5119.pdf

在原帖中查看解决方案

0 项奖励
回复
2 回复数
713 次查看
Irene
NXP Pro Support
NXP Pro Support

There is an application note on our website that might help answer some questions for you. 

https://www.nxp.com/docs/en/application-note/AN13329.pdf

0 项奖励
回复
666 次查看
yipingwang
NXP TechSupport
NXP TechSupport

There is a SerDes Validation tool which can be used to send raw data over the interface. You can loop back at near end or far end (if your link partner supports) and check if the bit stream is received correctly.

https://www.nxp.com/docs/en/user-guide/QCVS_SerDes_User_Guide.pdf
https://www.nxp.com/docs/en/application-note/AN5119.pdf

0 项奖励
回复