QSPI driver dosent work with s25fl164k ? I am using sdk 1.8.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

QSPI driver dosent work with s25fl164k ? I am using sdk 1.8.

2,771 Views
dhruvalkumarpat
Contributor III

My board design is based on ls1021aiot board . I have ls1020a on board and with different qspi flash chip than on ls1021aiot board.

QSPI flash part on our board "s25fl164k" . WIth existing driver I was able to perform "Erase" operation . I am not sure about write but "READ" is deffinately not working as it crashes my system when I try to read a mtd partition. I have done following changes at driver and device tree to work for my "qspi " flash part.

Changes in device tree :

kernel/3.12/arch/arm/boot/dts/

&qspi {

        num-cs = <2>;

        bus-num = <0>;

        fsl,spi-num-chipselects = <2>;

        fsl,spi-flash-chipselects = <0>;

        status = "okay";

        qflash0: s25fl164k@0 {

                #address-cells = <1>;

                #size-cells = <1>;

                compatible = "spansion,s25fl164k", "jedec,spi-nor";

                spi-max-frequency = <20000000>;

                reg = <0>;

                m25p,fast-read;

                partition@0 {

                        label = "rcw";

                        reg = <0x0 0x1000>;

                };

                partition@1 {

                        label = "u-boot";

                        reg = <0x10000 0x100000>;

                };

                partition@3 {

                        label = "environment";

                        reg = <0x110000 0x600000>;

                };

        };

};

Changes in kernel driver

kernel/3.12/drivers/mtd/spi-nor/spi-nor.c I added following line of code in device list structure .

{ "s25fl164k",  INFO(0x014017,      0,  64 * 1024, 128, SECT_4K) },

What else Do I need to do to make this qSPI flash work ? Am I missing something ?  I habe my u-boot environment stored in qspi flash and I want to access them from linux using fw_printenv and fw_setenv . I will appreciate your help.

Thanks

Dhruval

Labels (1)
4 Replies

1,721 Views
andrewwozniak
Contributor II

Hello Dhruval,

We had a similar failure as indicated at bootup:

[  2.260106] m25p80 spi0.0: found s25fl116k, expected s25fl164k   <---
[  2.266301] m25p80 spi0.0: s25fl116k (2048 Kbytes)   <---
[  2.271246] 3 ofpart partitions found on MTD device spi0.0
[  2.276823] Creating 3 MTD partitions on "spi0.0":
[  2.281668] 0x000000000000-0x0000000c0000 : "U-Boot"
[  2.302309] 0x0000000c0000-0x0000000c2000 : "env"
[  2.321337] 0x0000000d0000-0x000000800000 : "Data0"
[  2.326397] mtd: partition "Data0" extends beyond the end of device "spi0.0" -- size truncated to 0x130000

One potential issue is that the Cypress S25FL164K device does not identify itself properly. I have seen some success by swapping its id 0x014017 with 0x014015 at spi-nor.c driver:

{ "s25fl116k",  INFO(0x014017,  0,  64 * 1024,  32, SECT_4K | SPI_NOR_DUAL_READ | SPI_NOR_QUAD_READ) },
{ "s25fl132k",  INFO(0x014016,  0,  64 * 1024,  64, SECT_4K) },
{ "s25fl164k",  INFO(0x014015,  0,  64 * 1024, 128, SECT_4K | SPI_NOR_DUAL_READ | SPI_NOR_QUAD_READ) },
{ "s25fl204k",  INFO(0x014013,  0,  64 * 1024,   8, SECT_4K | SPI_NOR_DUAL_READ) },

It now reports the proper size:

[    2.250171] m25p80 spi0.0: found s25fl164k
[    2.256368] m25p80 spi0.0: s25fl164k (8192 Kbytes)   <--- woohoo!

Additional investigation and testing is need to verify that there is an issue with 8Mbyte device identification.

Good luck,

Andrew

1,721 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Dhruval,

Please try whether QSPI flash can be read/write under u-boot with the following commands first, they decide whether this is Kernel driver problem.

=> sf probe 0:0

SF: Detected S25FL128S_64K with page size 256 Bytes, erase size 64 KiB, total 16 MiB

=> sf erase 0 100000

SF: 1048576 bytes @ 0x0 Erased: OK

=> sf write 82000000 0 1000

SF: 4096 bytes @ 0x0 Written: OK

=> sf read 81100000 0 1000

SF: 4096 bytes @ 0x0 Read: OK

=> cm.b 81100000 82000000 1000

Total of 4096 byte(s) were the same


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,721 Views
dhruvalkumarpat
Contributor III

Thanks for Replying.

Firstly, I have u-boot and rcw stored in QSPI and I can access qspi flash from u-boot and currently I am booting(u-boot) from same QSPI flash.

Secondly I am using different QSPI flash part(s25fl164k), Dose the linux driver support this part? As mentioned earlier I have tried to add support as I learn but it didn't seem to work for me at linux. Can you please guide me here.

Thanks

Dhruval

0 Kudos
Reply

1,721 Views
dhruvalkumarpat
Contributor III

Following changes in spi-nor.c  solved my problem .

{ "s25fl164k",  INFO(0x014017,      0,  64 * 1024, 128, SECT_4K | SPI_NOR_DUAL_READ | SPI_NOR_QUAD_READ) },

Thanks

Dhruval