Hi,
We are using a custom basic bootloader on the LS1046ARDB. We find on our board that copying an 8MB Application from the QSPI Flash to DDR RAM takes about 48s, which works out to ~ 0.16 MB/sec (using a standard implementation of the memcpy function)
Are these in line with expected speeds?
How can we check the current "mode" (Single, dual, quad modes of operation, as mentioned in Section 27.2.1 of the LS1046ARM Ref Manual) of the QSPI Flash?
We changed SCFG_QSPI_CFG[CLK_SEL] value to 0x4 (highest working value) to change the QSPI Clock divider value to 20, and found a moderate improvement in speed. The copy time for the same 8MB file came down to 30s, working out to ~ 0.26 MB/sec. Please suggest any other modifications/ configurations we can look at to further speed up QSPI Flash Read speeds.
Thanks,
Shivesh
LUT0
INSTR0; PAD0; OPRND0 - 0x0413
INSTR0 - 1 (it is CMD); PAD0 - 00; OPRND0 - 0x13
It means:
CMD - the first operation is send command
length of command 1 byte
value of this command is 0x13
INSTR1; PAD1; OPRND1 - 0x0820
INSTR1 - 2 (it is ADDR); PAD0 - 00; OPRND0 - 0x20
It means:
ADDR for QSPI operations
length of address is 32bits (0x20)
Have a great day,
Pavel Chubakov
Hi Pavel,
We tried using the default values however it is causing the flash to be read incorrectly. Below are the LUT0, LUT1 default values being programmed by our Lauterbach Debugger that read correctly -
LUT0 - 0x08200413 (default value mentioned in LS1046ARM : 0x08180403)
LUT1 - 0x24001C08 (default value mentioned in LS1046ARM : 0x24001C08)
Can you suggest any modifications to these that won't cause incorrect reads?
Check LUT setting in your bootloader. See the Sections 27.4.2.30 and 27.6.3.1 in the LS1046a Reference Manual:
https://www.nxp.com/webapp/Download?colCode=LS1046ARM
Have a great day,
Pavel Chubakov
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello Yiping, NXP community
Request you to respond to the above question. For us startup time is very important and QSPI speed is crucial to achieve required timing, your response will help us greatly.
yiping wang
Thanks
Chitra Amzarewale