LSDK2108 LS1012ARDB NOR Flash Layout

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LSDK2108 LS1012ARDB NOR Flash Layout

Jump to solution
890 Views
Hugh512
Contributor III

With my custom board, a 32M NOR flash is used. I want to change the layout.

LS1012ARDB flash layout

FlashLayout_old.PNG

Below is my expected NOR flash layout:
FlashLayout_expected.PNG

After I erase the NOR Flash and burn the images, System can't enter into uboot, it stops at PBL stage, Could you help to tell me what I should do to change my flash layout?

0 Kudos
1 Solution
826 Views
Oswalag
NXP TechSupport
NXP TechSupport

I see in your expected NOR flash layout that the actual size for u-boot environment is 262,144 but the size of memory for u-boot is only 256k, you also said that you modify lsdk2108_yocto_tiny_LS_arm64.itb to make it smaller and It works fine, Where did you test it?

View solution in original post

0 Kudos
4 Replies
827 Views
Oswalag
NXP TechSupport
NXP TechSupport

I see in your expected NOR flash layout that the actual size for u-boot environment is 262,144 but the size of memory for u-boot is only 256k, you also said that you modify lsdk2108_yocto_tiny_LS_arm64.itb to make it smaller and It works fine, Where did you test it?

0 Kudos
788 Views
Hugh512
Contributor III

Thank you, Oswalag.

Uboot has at least 1M size, but I made a mistake, only reserved only 1M, After I reserved 1.5M, the start address of uboot environment changed to 0x280000, it works.

870 Views
Oswalag
NXP TechSupport
NXP TechSupport

If you try to use the same LS1012ARDB flash layout on your custom board works fine?

0 Kudos
864 Views
Hugh512
Contributor III

LS1012ARDB default NOR Flash Size is 64M, My custom board NOR Flash size is 32M, I modifiy lsdk2108_yocto_tiny_LS_arm64.itb to make it smaller. It works fine. After I relocated the pfe_fw_sbl.itb to 0x001C 0000(256K size) in NOR Flash, It's not work. 

0 Kudos