I am working on generating the new kernel tarball with custom kernel to replace exit kernel on target board.
I followed the suggestion on page. 174 (Layerscape Software Development Kit User Guide, LSDK 20.04_290520) "How to replace the default Linux kernel with custom kernel on target board".
The steps are:
1) flex-builder -c linux:custom -a arm64
2) flex-builder -c linux -a arm64
3) flex-builder -i mkbootpartition -a arm64
then, a new kernel tarball "<flexbuild-dir>/build/image/linux_5.4_LS_arm64_<timestamp>.tgz" should be generated, but it does not.
The result is showed as below,
Which step do I miss ?
Note,
On the LSDK 19.09, the kirnel tarball could be generated correctly.
Thanks
It is a mistake in LSDK 2004 User Guide.
Correct statement is the follow:
The new kernel tarball <flexbuild-dir>/build/images/bootpartition_LS_arm64_lts_5.4_<timestamp>.tgz will be generated.
Have a great day,
Pavel Chubakov