I debugging LS1043ardb development board .U-boot have ls1043ardb_pbi.cfg file ,Details are as follows:
#Configure Scratch register
09570600 00000000
09570604 10000000
#Alt base register
09570158 00001000
#Disable CCI barrier tranaction
09570178 0000e010
09180000 00000008
#USB PHY frequency sel
09570418 0000009e
0957041c 0000009e
09570420 0000009e
#flush PBI data
096100c0 000fffff
Please help provide PBI related documents.
已解决! 转到解答。
16100c0 - refer to the LS1043A RM, Table 27-5. Description of PBL commands, Wait
1570178 - hidden CCI CONFIG register (additional information can be obtained by creating a Technical Case - refer to the https://community.freescale.com/thread/381898)
General description of the PBI commands is provided in the QorIQ LS1043A Reference Manual, Chapter 27 Pre-Boot Loader (PBL).
Please note that default PBL base address offset is 0x100_0000 and this offset is concatenated with 24-bit SYS_ADDR of a PBI command.
Decoding example:
09570600 00000000
ACS=0
BYTE_CNT=000100 (4 bytes)
CNT=1
SYS_ADDR=570600
Complete CCSR address with offset: 0x1570600 (SCFG_SCRATCHRW0)
Thank you request my problem.
I want to know PBI configure all hardware resource.
I study ls1043ardb_pbi.cfg file.I don't find 0x16100c0 0x1570178 register declaration in LS1043A Reference Manual.
16100c0 - refer to the LS1043A RM, Table 27-5. Description of PBL commands, Wait
1570178 - hidden CCI CONFIG register (additional information can be obtained by creating a Technical Case - refer to the https://community.freescale.com/thread/381898)