LS1043ARDB  DDR4 validation failed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1043ARDB  DDR4 validation failed

1,908 Views
hawkin
Contributor II

I make  DDR4 validation on LS1043ARDB by CodeWarrior QCVS, DDR controller register value get from u-boot-2016.11, But all validation failed. Failed tips: DDR initalization failed: D_INIT was not cleared by hardware!

Is CodeWarriro config error or register config error? Can you give me a right config project that used in CodeWarrior Development Studio for QorIQ LS series.

Original Attachment has been moved to: LS1043A_v1_0_codewarrior_regs.regs.zip

Labels (1)
Tags (1)
0 Kudos
2 Replies

1,163 Views
sureshk
Contributor II

Hi 张洪军 张 ,\

   I also have encountered same issue..

when i run the validation it was showing error like:

 

Error configuring the target! - DDR initialization failed: D_INIT was not cleared by hardware!>>

https://community.nxp.com/message/973994 

How didi you resolve this issue? Help me in this ..

Regards,

 suresh

0 Kudos

1,162 Views
addiyi
NXP Employee
NXP Employee

How did you get the value of DDR regs from UBoot? The easy way to to that is to stop uboot at prompt then from QCVS to use Import From Target (You can find this option under File format in Import tab).

Also, as a reference you can use attached configuration for LS1043ARBD (got to Import tab, select File format Annotated Hex Text and import the file).

Adrian

0 Kudos