LS1043A SPI and eSDHC Chip Select Conflict

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1043A SPI and eSDHC Chip Select Conflict

695件の閲覧回数
ian_m
Contributor I

It seems that the designated chip select pins for the SPI interface are muxed with the DATA[4:7] pins for the eSDHC interface, which means I can't use the eSDHC interface in 8-bit mode to connect to an eMMC if I also want SPI device(s)...?

Do I really have to sacrifice ~50% of my eMMC throughput to use an SPI device, or is there some way of assigning an unused GPIO pin for use as SPI Chip Selects? 

 

Ian

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 返信

680件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Customer can use 4-bit mode of eSDHC interface if they are using SPI and eSDHC simultaneously.

Each of the muxed pins cannot be independently configured therefore we cannot assign an unused GPIO pin for SPI Chip Selects

 

0 件の賞賛
返信