LS1027A - SD card boot

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LS1027A - SD card boot

48 次查看
Mietto
Contributor I

Hello,

We have developed a custom board with the LS1027A, but we can't get it to boot with the SD Card.

The LS1027A is set to 1.8V at the EVDD pin, meaning the SDIO interface is always at 1.8V, unlike the NXP dev kit, which is set to 3.3V. Then, in our board, we have a 1.8V/3.3V level translator to interface with the SD card, but that should be transparent to the LS1027A.

We can see activity in and out from the SD card, but the boot stops at some point.

Is the LS1027A able to reliably boot from SD card when the interface is at 1.8V?

The question comes from the recommendation below, taken from AN12028.

ls1027a sd card.png

 Best regards.

0 项奖励
回复
1 回复

10 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Confirming with the AE team.

0 项奖励
回复