LS1023A and four KSZ8081

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1023A and four KSZ8081

1,044 Views
markclaus
Contributor I


Can the LS1023A be interfaced with four KSZ8081 10Base-T/100Base-TX Ethernet PHYs by sharing the EMI1_MDC/MDIO with two and EMI2_MDC/MDIO with the oter two PHYs? Not sure how to connect the KSZ8081 CRS_DV signals

Labels (1)
0 Kudos
1 Reply

824 Views
r8070z
NXP Employee
NXP Employee


Have a great day,

As I can see in the datasheet

http://ww1.microchip.com/downloads/en/DeviceDoc/KSZ8081MNX-RNB.pdf

KSZ8081 supports MII and RMII interfaces only. While the LS1023 does not support these interfaces. It supports hi-speed serial interfaces (SGMII, XFI …) and parallel RGMII interface which is not compatible to the MII/RMII. Consider using another PHY which has interface suitable for the LS1021A.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos