LS1021A SPI NOR MT25QU512ABB1EW9 Support

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LS1021A SPI NOR MT25QU512ABB1EW9 Support

647 次查看
ramkrishnan
Contributor III

I have a spi nor MT25QU512ABB1EW9 connected to the SPI2 Chip Select 2. What code would I use as a template in both u-boot as well as the linux kernel to support this. This particular chip is not supported in either. 

There is Quad SPI support in both for the ls1021a-twr but the spi-nor in my design in not used for bootup. There is a separate NOR flash that is used for bootup. 

Please let me know if you would like more details. 

Thank you,

Ram Krishnan

标签 (1)
标记 (3)
0 项奖励
回复
1 回复

545 次查看
Pavel
NXP Employee
NXP Employee

See the Section 7.15.2 of the SDK 2.0-1703 documentation:

https://www.nxp.com/docs/en/supporting-information/QORIQ-SDK-2.0-IC-REV0.pdf

 

This Section contains information about using dSPI driver on LS1021a-QDS board.

 

Have a great day,
Pavel Chubakov

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复