LS1021A PCIe Wifi Interface Issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LS1021A PCIe Wifi Interface Issue

446 次查看
jiye
Contributor V

Anyone knows what's the issue here.

My kernel does have the interface up

But after I scan there are no wifi names showing up

pastedImage_1.png

pastedImage_1.png

标签 (2)
标记 (2)
0 项奖励
1 回复

353 次查看
bpe
NXP Employee
NXP Employee

This is a  device-specific problem, which, based on the provided screen
captures, is a result of device's failure to respond to certain commands.
This is totally the driver and underlying HW specific, thus the suggestion
is to approach your radio card manufacturer for more detailed error output
interpretation and troubleshooting.


Have a great day,
Platon

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励