I am using LS1021A custom board with NOR flash (IS29GL256-70FLET) in IFC bus, so I need to calculate the IFC timing using the attached sheet which is provided by NXP, but when I use those values, the chip is not responding, that log I attached below, and the working log of reference board (LS1021A-TWR) attached here.
And I used the improper values in reference board configuration that log also same as custom board non working log. That means I am thinking the issue is in the timing values generated by the XL sheet,
Reference board improper values
=========================
#define CONFIG_SYS_NOR_FTIM0 (FTIM0_NOR_TACSE(0x1) | \
FTIM0_NOR_TEADC(0x1) | \
FTIM0_NOR_TAVDS(0x0) | \
FTIM0_NOR_TEAHC(0x20))
#define CONFIG_SYS_NOR_FTIM1 (FTIM1_NOR_TACO(0x1) | \
FTIM1_NOR_TRAD_NOR(0x3) | \
FTIM1_NOR_TSEQRAD_NOR(0x1))
#define CONFIG_SYS_NOR_FTIM2 (FTIM2_NOR_TCS(0x1) | \
FTIM2_NOR_TCH(0xe) | \
FTIM2_NOR_TWPH(0x0e) | \
FTIM2_NOR_TWP(0x23))
Reference board proper values
=======================
#define CONFIG_SYS_NOR_FTIM0 (FTIM0_NOR_TACSE(0x4) | \
FTIM0_NOR_TEADC(0x5) | \
FTIM0_NOR_TAVDS(0x0) | \
FTIM0_NOR_TEAHC(0x5))
#define CONFIG_SYS_NOR_FTIM1 (FTIM1_NOR_TACO(0x35) | \
FTIM1_NOR_TRAD_NOR(0x1A) | \
FTIM1_NOR_TSEQRAD_NOR(0x13))
#define CONFIG_SYS_NOR_FTIM2 (FTIM2_NOR_TCS(0x4) | \
FTIM2_NOR_TCH(0x4) | \
FTIM2_NOR_TWP(0x1c) | \
FTIM2_NOR_TWPH(0x0e))
Custom board used value
====================
#define CONFIG_SYS_NOR_FTIM0 (FTIM0_NOR_TACSE(0x1) | \
FTIM0_NOR_TEADC(0x1) | \
FTIM0_NOR_TAVDS(0x0) | \
FTIM0_NOR_TEAHC(0x20))
#define CONFIG_SYS_NOR_FTIM1 (FTIM1_NOR_TACO(0x20) | \
FTIM1_NOR_TRAD_NOR(0x13) | \
FTIM1_NOR_TSEQRAD_NOR(0x10))
#define CONFIG_SYS_NOR_FTIM2 (FTIM2_NOR_TCS(0x1) | \
FTIM2_NOR_TCH(0xe) | \
FTIM2_NOR_TWPH(0x0e) | \
FTIM2_NOR_TWP(0x23))
Please suggest me to resolve this issue.
Regards
Winston