Dear all,
I would like to know if it is possible to suspend to ram on the LS1021.
Also is frequency scaling possible?
Regards,
Dennis
Hello Dennis Wokke,
For your question about suspend to ram and frequency scaling on LS1021A, QorIQ-SDK-1.7 give below highlights in Section 1.3 What's new:
This pdf is available at:
http://www.freescale.com/files/soft_dev_tools/doc/support_info/QorIQ-SDK-1.7-IC-RevB.zip
Have a great day,
Lunmin
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Lunmin,
Maybe I should have been more clear on my objective.
I have the TWR-LS1021a board. In the documentation I have read that it will not do deep-sleep mode.
Also I read there was a silicon issue regarding power mangement, however I am unable to find the reference to this.
I want to use the LS1021a for un upcoming project, but can only use it if I am 100% certain I can get low power while the system is idle. It should go into deep sleep mode a lt of the time to preserve battery power. As I cannot test this on the TWR-LS1021a I'm at a loss.
Maybe you can give me some certainty about this.
I must say I had not seen the Rev B yet, and that looks promising.
Best regards,
Dennis