LS1020A/LS1021A QSPI Boot Speed Change in RCW

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LS1020A/LS1021A QSPI Boot Speed Change in RCW

510 次查看
christopheniclaes
Contributor I

I post this message in order to share our experience about issues with LS1020A QSPI Boot (also valid for LS1021).

The sample RCW files provided in LSDK all contain a command which change the divider for QSPI clock speed:

write 0x57015c, 0x00000803

Where does this value come from?

Explanation:

- It is a write to SCFG_QSPI_CFG

- As the endianess has not been setup yet, the value to be written is bit-flipped from what you can find in the reference manual.

- The value given in the RCW examples (0x00000803), when bit-flipped, is 0xC0100000:

- The "1" is a default value for bit 11

- The is a strange value since the high-order bit must be 0 as described in the reference manual.

- If we ignore the high-order bit (which is what the CPU seems to do), the divider value is 100 which correspond to PLL/20. I confirmed this divider with an oscilloscope.

- If we replace this value with 0x00000802 (the same but without the strange bit), the result is the same.

- I tested other values and all of them worked as expected

I hope this message will help others to setup the speed of their QSPI bus.

 

 

0 项奖励
回复
0 回复数