In the LS1043A is there any default Ethernet interface (like Ethernet Controller1(EC1) or EC2) that should be used for tftp programming?
Can any GPIO of LS1043A be used for giving pulse to an external Watchdog circuit or any dedicated GPIO is available for this purpose?
已解决! 转到解答。
Primary Ethernet interface is defined in the board's header file, for example "ls1043ardb.h":
as
#define CONFIG_ETHPRIME "FM1@DTSEC3"
GPIOs can be used according to the board's designer needs.
Primary Ethernet interface is defined in the board's header file, for example "ls1043ardb.h":
as
#define CONFIG_ETHPRIME "FM1@DTSEC3"
GPIOs can be used according to the board's designer needs.