IEEE 1588v2 and LS1021A

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IEEE 1588v2 and LS1021A

Jump to solution
1,661 Views
jamessun
Contributor I

Regarding the IEEE 1588v2 support by LS1021A, it is supported for all THREE Ethernet Controllers simultaneously?

Labels (1)
0 Kudos
Reply
1 Solution
1,449 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello James Sun,

LS1021 processor provides hardware assist for IEEE 1588 protocal. IEEE 1588 compliant time stamping on the device is accomplished using the per-port transmit time stamping registers with each Ethernet controller memory space, all TSEC  can use this assistance in the same way and use hardware time-tamp mechanism simultaneously.

Please note common 1588 time stamping registers exist within the eTSEC1 memory space, the eTSEC1 controller must remain enabled in order to use 1588 time stamping for any Ethernet port.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,450 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello James Sun,

LS1021 processor provides hardware assist for IEEE 1588 protocal. IEEE 1588 compliant time stamping on the device is accomplished using the per-port transmit time stamping registers with each Ethernet controller memory space, all TSEC  can use this assistance in the same way and use hardware time-tamp mechanism simultaneously.

Please note common 1588 time stamping registers exist within the eTSEC1 memory space, the eTSEC1 controller must remain enabled in order to use 1588 time stamping for any Ethernet port.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply