IEEE 1588v2 and LS1021A

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

IEEE 1588v2 and LS1021A

跳至解决方案
1,684 次查看
jamessun
Contributor I

Regarding the IEEE 1588v2 support by LS1021A, it is supported for all THREE Ethernet Controllers simultaneously?

标签 (1)
0 项奖励
回复
1 解答
1,472 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Hello James Sun,

LS1021 processor provides hardware assist for IEEE 1588 protocal. IEEE 1588 compliant time stamping on the device is accomplished using the per-port transmit time stamping registers with each Ethernet controller memory space, all TSEC  can use this assistance in the same way and use hardware time-tamp mechanism simultaneously.

Please note common 1588 time stamping registers exist within the eTSEC1 memory space, the eTSEC1 controller must remain enabled in order to use 1588 time stamping for any Ethernet port.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,473 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Hello James Sun,

LS1021 processor provides hardware assist for IEEE 1588 protocal. IEEE 1588 compliant time stamping on the device is accomplished using the per-port transmit time stamping registers with each Ethernet controller memory space, all TSEC  can use this assistance in the same way and use hardware time-tamp mechanism simultaneously.

Please note common 1588 time stamping registers exist within the eTSEC1 memory space, the eTSEC1 controller must remain enabled in order to use 1588 time stamping for any Ethernet port.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复