What settings are needed to use UART3/4 with LX2160ardb_rev2?
A two-way RS232C adapter cable was created according to the "QorIQ LX2160A Reference Design Board Reference Manual". We further considered it necessary to set RCW and set UART1/UART2_RTSCTS_PMUX to 0b010.
I believe all that is left is to set up the same as UART1/2, but UART3/4 is not responding.
Is there something else that needs to be set up?
已解决! 转到解答。
Explanation was insufficient.
I am developing software that runs on lx2160ardb_rev2 and in it I want to use all channels of UART1/2/3/4 simultaneously.
>Please add the following definition in plat/nxp/soc-lx2160a/lx2160ardb/plat_def.h.
>#define NXP_UART_ADDR 0x021E0000
>Or
>#define NXP_UART_ADDR 0x021F000
I think this method is a change to make if you want to switch the UART channel used by uboot.
The reference manual does not explain what parameters I need to set if I want to use UART3/4. What parameters other than UART registers must be changed?
Except configuring RCW UART1/UART2_RTSCTS_PMUX as 0b010.
You also need to modify ATF source code to make it support UART3/4.
Please go to ATF source code folder flexbuild_lsdk2108/components/firmware/atf,
Please add the following definition in plat/nxp/soc-lx2160a/lx2160ardb/plat_def.h.
#define NXP_UART_ADDR 0x021E0000
Or
#define NXP_UART_ADDR 0x021F0000
Then rebuild ATF images and deploy them on the target board.
Explanation was insufficient.
I am developing software that runs on lx2160ardb_rev2 and in it I want to use all channels of UART1/2/3/4 simultaneously.
>Please add the following definition in plat/nxp/soc-lx2160a/lx2160ardb/plat_def.h.
>#define NXP_UART_ADDR 0x021E0000
>Or
>#define NXP_UART_ADDR 0x021F000
I think this method is a change to make if you want to switch the UART channel used by uboot.
The reference manual does not explain what parameters I need to set if I want to use UART3/4. What parameters other than UART registers must be changed?
I found the cause.
The diagram in the "QorIQ LX2160A Reference Design Board Reference Manual" is incorrect. The IN/OUT signal connections for UART3/4 are listed in reverse.
In the figure, the wiring between DB9F and UART3/4 is described as follows.
In other words, the OUT signal is connected to pin 2 and the IN signal to pin 3 in DB9M of UART3/4.
In contrast, the UART1/2 connections are reversed. The IN signal is on pin 2 and the OUT signal on pin 3.
In other words, the cable is described in this figure so that the IN/OUT signals are reversed for UART1/2 and UART3/4.
The solution is simple. Use a cross cable for UART1/2 and a straight cable for UART3/4, or wire either IN/OUT line opposite to the diagram.