Hi
We use SDK: Freescale Linux LS1021A SDK v0.4
We created the tool-chain with Yocto:
$ bitbake fsl-toolchain
The tool-chain works. We can to compile the codes.
Now I would like to add the libxml2 library in the toolchain in order to use this library during linking.
The libxml2-2.9.1.tar.gz file is in the <SDK>/source folder.
How can I add the libxml2 library to the toolchain?
Regards
Victor
解決済! 解決策の投稿を見る。
Hello Victor,
Please run "bitbake libxml2", and the libraries which you required are deployed in build_ls1021atwr_release/tmp/sysroots/ls1021atwr/usr/lib/.
Have a great day,
Yiping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello Victor,
Please run "bitbake libxml2", and the libraries which you required are deployed in build_ls1021atwr_release/tmp/sysroots/ls1021atwr/usr/lib/.
Have a great day,
Yiping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thank you Yiping,
I copied the all libxml2.* files from the build_ls1021atwr_release/tmp/sysroots/ls1021atwr/usr/lib/ folder to
the folder /opt/fsl-networking/QorIQ-SDK-V1.8/sysroots/cortexa7hf-vfp-neon-fsl-linux-gnueabi/usr/lib folder and also added /libxml folder to /usr/include/ .
Regards
Victor