How to set lx2160 in pcie endpoint mode?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to set lx2160 in pcie endpoint mode?

1,088件の閲覧回数
peiqiongye
Contributor II

When I tried to set lx2160 in pcie endpoint mode, pci_epf_test driver cannot setup. 

Using LSDK 21.08.

my reference:

https://community.nxp.com/t5/QorIQ-Knowledge-Base/LS1046A-RDB-in-PCIe-Endpoint-Mode/ta-p/1107415

Detal steps as below:

1. RCW config: set HOST_AGT_PEX1 to HOST_AGT_PEX6 as 1.

2. kenel dts:

pcie_ep5pcie_ep@3800000 {
            compatible = "fsl,lx2160a-pcie-ep";
            reg = <0x00 0x03800000 0x0 0x00100000
                   0xa0 0x00000000 0x8 0x00000000>;
            reg-names = "regs""addr_space";
            interrupts = <GIC_SPI 128 IRQ_TYPE_LEVEL_HIGH>, /* AER interrupt */
                     <GIC_SPI 128 IRQ_TYPE_LEVEL_HIGH>, /* PME interrupt */
                     <GIC_SPI 128 IRQ_TYPE_LEVEL_HIGH>; /* controller interrupt */
            interrupt-names = "aer""pme""intr";
            apio-wins = <256>;
            num-lanes = <8>;
            num-ib-windows = <24>;
            num-ob-windows = <256>;
            max-functions = /bits/ 8 <2>;
            status = "disabled";
        };

 

3. kconfig:

#
# PCI Endpoint
#
CONFIG_PCI_ENDPOINT=y
CONFIG_PCI_ENDPOINT_CONFIGFS=y
CONFIG_PCI_EPF_TEST=y 

 

4. add pci_epf_test device.

cd /sys/kernel/config/pci_ep/
mkdir functions/pci_epf_test/func1
echo 0x1957 > functions/pci_epf_test/func1/vendorid
echo 0x8d80> functions/pci_epf_test/func1/deviceid
echo 16 > functions/pci_epf_test/func1/msi_interrupts
echo 8 > functions/pci_epf_test/func1/msix_interrupts
echo 0 > functions/pci_epf_test/func1/revid
ln -s functions/pci_epf_test/func1 controllers/3800000.pcie_ep
echo 1 > controllers/3800000.pcie_ep/start

After that, in RC side, cannot find EP driver via lspci command.

Maybe the reason is EPF DMA channel init faild, beacuse dma_request_chan_by_mask returned with "-EPROBE_DEFER" error. The dma_device_list is empty.

 

peiqiongye_1-1656558485750.png

Can someone show me how to set lx2160 pcie as endpoint mode?

タグ(3)
0 件の賞賛
1 返信

1,057件の閲覧回数
kenli
NXP Employee
NXP Employee

Is this verified with LX2160ARDB ? if so,pls refer to the LSDK user guide below
"7.2.8.4 PCIe Endpoint Mode Linux driver"

Best regards
0 件の賞賛