Hi,
On LS1043ardb board, when the CPU running on 64-bit mode, I can bring up the secondary core by bellow:
u64 r[7] = {0};
r[0] = 0xC4000003;
r[1] = cpuId;
r[2] = kernelAddr;
SMC #0
However, when I run the CPU on 32-bit compatible mode, I cannot bring up the secondary core after changing above u64 to u32, and r[0] to 0x84000003.
Is there any suggestions to enable SMP on 32-bit compatible mode?
Thanks.