How to enable RSTP

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to enable RSTP

7,480 次查看
rpk
Contributor II

Hi!

We have developed a custom board with a LS1028. The switch ports are added to a bridge (br0), and the bridges of multiple boards are daisy chained together in a ring. STP (Spanning Tree Protocol) is enabled to support the ring configuration. The recovery time of STP is way too long, and we need to enable RSTP instead. How do we do this, and how do we optimise for a shortest possible recovery time ?

To configure STP we simply use brctl (for example "brctl stp br0 on"). 

We are using LS SDK 20.04 v4.19.

Any help is greatly appreciated. Thanks

/Rolf

标签 (1)
标记 (3)
4 回复数

7,386 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Please switch the bridge mode from stp to rstp using the mstpctl application.

mstpctl setforcevers br0 rstp

Please refer to 4.4. RSTP — Processor SDK Linux Documentation 

GitHub - mstpd/mstpd: Multiple Spanning Tree Protocol Daemon 

7,386 次查看
rpk
Contributor II

We have experimented with mstpd / mstpctl now. The results are much better, but we need even better results.

The minimum values we were able to set are:

mstpctl sethello br0 1

mstpctl setmaxage br0 6

mstpctl setfdelay br0 4

mstpctl setageing br0 10

This results in a recovery time of roughly maximum 6 seconds. Afaik the maximum should be around 3 x hello time, but we are seeing around twice this in practice.

Anyways, our ultimate goal is sub-second recovery time. 

All our bridges are of same priority and the devices must be able to reconnect in any fashion (ring, mesh, star) without disturbing multicast ip6 traffic for too long (ideally sub second). How do we accomplish this?

0 项奖励
回复

7,386 次查看
rpk
Contributor II

Thanks. We will try this.

But what we were hoping is that RSTP would be performed solely at L2 level with such a powerful switch as the one in LS1028. Using a daemon gives the impression that this is performed at application level?

/Rolf

0 项奖励
回复

5,834 次查看
Shinra
Contributor II

I'm currently having the same thoughts, any new clues about the matter ?

P.

0 项奖励
回复