How can lx2160a control the GPIO3[3] in uboot ?
I want to control GPIO3[3] of lx2160a, but can not set GPIO3 high or low.
1:
I have added setting to RCW
IRQ03_00_PMUX=1
EVT43_PMUX=1
EVT20_PMUX=1
2
use GPIO3[3] to generate a signal of PCIE card reset;
so I add the code to UBOOT:
#define GPIO3_BASE_ADDR 0x2320000
u32 val = 0x00000008;
u32 tmp = 0;
readsl(GPIO3_BASE_ADDR, &tmp, 1);
val = val | tmp;
writesl(GPIO3_BASE_ADDR, &val, 1);
readsl(GPIO3_BASE_ADDR + 0x4, &tmp, 1);
val = 0x00000008;
val = tmp & (~val);
writesl(GPIO3_BASE_ADDR + 0x4, &val, 1);
readsl(GPIO3_BASE_ADDR + 0x8, &tmp, 1);
val = 0x00000008;
val = tmp & (~val);
writesl(GPIO3_BASE_ADDR + 0x8, &val, 1);
udelay(1000*20);
val = 0x00000008;
val = tmp | val;
writesl(GPIO3_BASE_ADDR + 0x8, &val, 1);
3 after rebuild the uboot, and load the bin to SD card, I reset the lx2160a board,
find that value of GPIO3[3] is always 0
=> md.l 0x2320000
02320000: 00000008 00000000 00000000 00000000 ................
4
manual control GPIO3[3] under uboot command, also can not control
mw 0x2320008 0x8
return vale also is :
=> md.l 0x2320000
02320000: 00000008 00000000 00000000 00000000 ................
5 so How can lx2160a control the GPIO3[3] in uboot ?
thanks
mw 2320008 FFFFFFFF
md 2320000
02320000: ffffffff 00000000 ff0f8000 ff0f8000 ................
02320010: 00000000 00000000 ffffffff 00000000 ................
02320020: 00000000 00000000 00000000 00000000 ................
mw 2320008 0
md 2320000
02320000: ffffffff 00000000 00000000 ff0f8000 ................
02320010: 00000000 00000000 ffffffff 00000000 ................
02320020: 00000000 00000000 00000000 00000000 ................
Please provide the processor connection schematics as PDF for inspection and explain where/how the GPIO3[3] is probed.
Also please consider that U-Boot operates in big-endian - i.e. for the GPIO3[3] corresponding bit is 0x10000000.
please refer the attach file ... also can not control GPIO3[3]
mw 2320008 FFFFFFFF
md 2320000
02320000: ffffffff 00000000 ff0f8000 ff0f8000 ................
02320010: 00000000 00000000 ffffffff 00000000 ................
02320020: 00000000 00000000 00000000 00000000 ................
mw 2320008 0
md 2320000
02320000: ffffffff 00000000 00000000 ff0f8000 ................
02320010: 00000000 00000000 ffffffff 00000000 ................
02320020: 00000000 00000000 00000000 00000000 ................
GPIO should be enabled in the GPIBE register - refer to the QorIQ LX2160A Reference Manual, 20.5.1.7 GPIO Input Buffer Enable Register (GPIBE).
Please provide U-Boot booting log as textual attachment.
=> md 2320000
02320000: 00000000 00000000 00000000 00000000 ................
02320010: 00000000 00000000 00000000 00000000 ................
02320020: 00000000 00000000 00000000 00000000 ................
=> mw 2320000 FFFFFFFF
=> md 2320000
02320000: ffffffff 00000000 00000000 00000000 ................
02320010: 00000000 00000000 00000000 00000000 ................
02320020: 00000000 00000000 00000000 00000000 ................
=> mw 2320008 FFFFFFFF
=> md 2320000
02320000: ffffffff 00000000 00000000 00000000 ................
02320010: 00000000 00000000 00000000 00000000 ................
02320020: 00000000 00000000 00000000 00000000 ................
=> mw 2320018 FFFFFFFF
=> md 2320000
02320000: ffffffff 00000000 ff0f8000 ff0f8000 ................
02320010: 00000000 00000000 ffffffff 00000000 ................
02320020: 00000000 00000000 00000000 00000000 ................
=> mw 2320008 FFFFFFFF
=> md 2320000
02320000: ffffffff 00000000 ff0f8000 ff0f8000 ................
02320010: 00000000 00000000 ffffffff 00000000 ................
02320020: 00000000 00000000 00000000 00000000 ................
=> mw 2320008 0
=> md 2320000
02320000: ffffffff 00000000 00000000 ff0f8000 ................
02320010: 00000000 00000000 ffffffff 00000000 ................
02320020: 00000000 00000000 00000000 00000000 ................