Hi all,
In the "16.4.13.10 Rewriter" chapter of [1], it mentions:
The device includes a rewriter common for all ports that determines how the egress frame is edited before transmission. The rewriter performs the following editing:
So, my question is how can I enable these functions in OpenIL1.7.1 for ls1028ardb?
Thanks,
Yi
[1]Lsa, A. (2019). QorIQ LS1028A Reference Manual.
Hi Yiping,
I want to use ls1028ardb to translate traffic flows to/from TSN streams which is identified by {DstMAC, VLAN}. So it may need to touch MAC address rewriting and VLAN tag rewriting. Is that possible?
Thanks,
Yi
Please refer to the following feedback from the LSDK development team.
As for frame rewriting, the switch has limited MAC address rewriting abilities, basically only swapping of source MAC and destination MAC. I don't think we'll support that soon in the Linux driver. We'll try to support, however, VLAN ID and PCP rewriting.
Please configure Linux Kernel as the following.
Symbol: TSN [=y]
│ Type : boolean
│ Prompt: 802.1 Time-Sensitive Networking support
│ Location:
│ -> Networking support (NET [=y])
│ -> Networking options
│ Depends on: NET [=y] && VLAN_8021Q [=y] && PTP_1588_CLOCK [=y]