GPIO pins on LS1046ARDB

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

GPIO pins on LS1046ARDB

864 次查看
andreasr
Contributor I

Are there any GPIO pins available on the LS1046ARDB? 

I didn't find anything about it in the getting started guide or the reference manual.

I know, that the LS1046A comes with a GPIO module, but there seems to be no pin available on the RDB connected to a GPIO port.

标签 (1)
0 项奖励
1 回复

570 次查看
r8070z
NXP Employee
NXP Employee


Have a great day,

As I could see in the LS1046ARDB schematics there are not pins dedicated for GPIO. According to the LS1046A manual all pins used by the GPIO modules are shared with other peripheral controllers. The RDB uses most of those controllers. You may create technical case with request for the LS1046ARDB schematics and check if you can use some pins as GPIO for your case. Please see How I could create a Techical Case? 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励