Failed to write memory

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Failed to write memory

2,102 次查看
bladerunner1010
Contributor III

I'm getting error via Codewarrior when trying to connect with flash programmer or when I run the initialization script.

Jtag connection seems OK and I am able to read the RCW.

Error is:

Failed to write memory at address 0x2016002c on core CortexA53#0.

Chip is LS1023A.

Thanks for your help

@yi 

标记 (2)
4 回复数

2,057 次查看
bladerunner1010
Contributor III

please attach your initialization script and will try to help 

0 项奖励

2,051 次查看
richardadams
Contributor III

I'm using the initialization script for the LS1043ARDB (LS1043A_RDB._init.py) with the following changes to support Hardcoding the RCW since  my board has a Blank NOR  Flash which will be my boot device when I can program it

USE_SAFE_RCW = True

BOOT_CHIP_SELECT = 2

The error is generated from Init_BRR when the line " DCSR_BE_M(0x16002C, 0x0000000E)" is executed

 

 

2,059 次查看
richardadams
Contributor III

I have the same error with a LA1043A board. Did anyone ever identify the cause of this error and how to work around it?

0 项奖励

2,084 次查看
shu-zyc1
Contributor II

l meet the same question ,how do you solve it 

thanks you

0 项奖励