Hi,
I followed exactly what the lsdk1906 to tell me enable necessary modules and also in the device tree file my in my device it shows me this error when I use:
modprobe g_ether
Failed to get clk "ref:-2
Anyone knows why?
Hello Elias Bitbaker,
Please refer to Linux Kernel definition
USB Gadget support --->
<M> USB Gadget functions configurable through
configfs
<M> USB Gadget precomposed configurations
<M> Ethernet Gadget (with CDC Ethernet support)
Please refer to the device tree definition
usb0: usb3@2f00000 {
compatible = "snps,dwc3";
reg = <0x0 0x2f00000 0x0 0x10000>;
interrupts = <0 60 0x4>;
dr_mode = "peripheral";
snps,quirk-frame-length-adjustment = <0x20>;
snps,dis_rxdet_inp3_quirk;
maximum-speed = “super-speed”;
};
Please insmod related ko modules as the following.
# insmod libcomposite.ko
# insmod u_ether.ko
# insmod usb_f_ecm.ko
# insmod usb_f_ecm_subset.ko
# insmod usb_f_rndis.ko
# insmod g_ether.ko
Thanks,
Yiping
Hi Yiping,
I did all the steps but I see this
And my device tree file is like this below:
(1)Do you know what's wrong here, it seems like my PC does not detect the device.
(2)Also do I need to ensure the UDC USB controller?
(3) I believe the USB2.0 is back compatible with the USB3.0, if I just plug into a USB2.0 port am I suppose to use the same configuration in the device tree and kconfig? Please help this is really important to me.