Hello community,
p1044 of LSDKUG_Rev20.04, it is written as follows.
According to these document, it seems to support TLS but not DTLS.
*****
The following can be offloaded in hardware in current SDK (not a complete list):
• SSL: TLS v1.1 & TLS v1.2 with one-shot cipher modes (a single ioctl for both encryption and authentication):
— AES128-SHA1
— AES256-SHA1
— AES128-SHA256
— AES256-SHA256
— Only supported on kernel version 4.19.
— Not supported on kernel version 5.4
— One shot cipher AES128-SHA1 and AES256-SHA1 for TLS1.0 is not any more supported.
*****
However, according to the LS1046A Security RM, it says:
It appears to support both TSL and DTLS here.
LS1046ASECRM Rev. 0, 05/2017 p366
******
9.2 SSL/TLS/DTLS record encapsulation and decapsulation overview
SEC supports the following versions of the TLS family of security protocols:
• SSL 3.0
• TLS 1.0
• TLS 1.1
• TLS 1.2
• DTLS 1.0 (a variant of TLS 1.1)
• DTLS 1.2 (a variant of TLS 1.2)
*****
My question is, does LS1046A w/LSDK20.04 support DTLS?
Best Regards,
Kanou
已解决! 转到解答。
Hello Kanou,
Though DTLS is a variant of TLS, it has never been tested by LSDK testing team.
I also confirm with LSDK development team, they don't know if DTLS is at all supported ever in LSDK.
LSDK 20.04 supports two kernel version – v4.19 and v5.3.
Moreover, do note a point that TLS is supported on Linux kernel 4.19 only.
Thanks,
Yiping
Hello Kanou,
Though DTLS is a variant of TLS, it has never been tested by LSDK testing team.
I also confirm with LSDK development team, they don't know if DTLS is at all supported ever in LSDK.
LSDK 20.04 supports two kernel version – v4.19 and v5.3.
Moreover, do note a point that TLS is supported on Linux kernel 4.19 only.
Thanks,
Yiping