Does LS1012A support Wi-Fi offload?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does LS1012A support Wi-Fi offload?

811件の閲覧回数
neilbullock
Contributor I

Does the LS1012A device support Wi-Fi offload in a similar manner to LS1024A, as shown in the attached diagram?

ラベル(1)
タグ(1)
0 件の賞賛
1 返信

634件の閲覧回数
Pavel
NXP Employee
NXP Employee

Wi-Fi is available for the LS1024. NXP ASK for the LS1024a supports Wi-Fi offload.

See the LS1024A Communications Processor Application Solution Kit - Fact Sheet:

http://www.nxp.com/assets/documents/data/en/fact-sheets/LS1024AASKFS.pdf


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛