DDR4 and ECC on LS1046

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

DDR4 and ECC on LS1046

1,585 次查看
Filippo
Contributor III

Hi all,

I'm approaching an LS1046 design, and I would like to use a non-ECC DDR4.

On the reference design ( sch-29142 ) there is the socket for a 288 pin ecc ddr4 dimm.

Can I avoid to use ECC, so using a 260 pin ddr4 module ?

Regards

Filippo

标签 (1)
标记 (2)
0 项奖励
2 回复数

1,283 次查看
r8070z
NXP Employee
NXP Employee


Have a great day,

Yes you can to use a non-ECC DDR4 memory. The DDR ECC is enabled in the DDR_SDRAM_CFG register.  

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励

1,252 次查看
atrqua
Contributor I

Have u met  a  NOTICE about DDR :NOTICE: UDIMM M4DS-AGS1QC0J-BE82  when boot LS1046 ?

Thank u

0 项奖励