Hi !
I used to use the SDK1.9 (LS1021a-twr) without any big issue, and now I'm trying to install the SDK2.0-1703 to update linux kernel, and I have some issues making it work, so I'd like to check if I'm doing things correctly. At the moment:
- I installed the SDK2.0 Source iso
- I installed the SDK2.0 Cache iso
- I installed the SDK2.0-1703 tgz file
- I triggered a fsl-image-full build
And I have quite a lot of errors. As a comparison, I just performed again a full build of the SDK1.9 without any issue.
So to be able to give more meaningful feedback, I'm starting a SDK2.0 SOURCE install, without cache or 1703. I'll update the thread when the installation is done.
So I'd like to know:
- is this way of doing things ok ?
- if I install and build only the SDK2.0 part, can I perform the SDK2.0-1703 update on an existing installation or should I clean it first ?
Best,
V.
已解决! 转到解答。
The SDK documentation recommends install CACHE iso before SOURCE iso.
Have a great day,
Pavel Chubakov
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
The SDK documentation recommends install CACHE iso before SOURCE iso.
Have a great day,
Pavel Chubakov
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Use Ubuntu 14.04 for SDK 2.0-1703. Do not use Ubuntu 16.
Usually use the following command sequence for SDK installing under Ubuntu 14.04:
Message: /bin/sh -> dash
Answer after password – No
Message:
Removing 'diversion of /bin/sh to /bin/sh.distrib by dash'
Adding 'diversion of /bin/sh to /bin/sh.distrib by bash'
Removing 'diversion of /usr/share/man/man1/sh.1.gz to /usr/share/man/man1/sh.distrib.1.gz by dash'
Adding 'diversion of /usr/share/man/man1/sh.1.gz to /usr/share/man/man1/sh.distrib.1.gz by bash'
Message: /bin/sh -> bash
Usually Linux recommends also run the following command: sudo usr/sbin/visudo
See also the following page in NXP community abut EULA:
https://community.nxp.com/thread/445051
Have a great day,
Pavel Chubakov
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------